Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M580 SD memory card format procedure
M580 CPU SD memory card format procedure
NOTE
- Only use the BMXRMS004GPF SD card for the M580
  1. Connect to M580 and make sure the Unity project is “Equal”, “Run” and “Built”
  2. Stop the PLC
  3. Open SD card door and make sure LED is ON
  4. Open the “Animation Table” Window
  5. Add system word %SW93.0 and %SW93.1
  6. Turn on the “Modification” button
  7. Enter value “1” for %SW93.0
  8. (This will start the format of the SD card then that value will change back to “0” and the value of %SW93.1 will go from “0” to “1” to indicate the format has completed successfully), (Formatting a standard SD card takes about 30-50 seconds)
  9. When completed, enter a value of “0” for both %SW93.0 and %SW93.1
  10. Start PLC