Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity Pro, How to keep eds DTM in the DTM catalog when updating Unity Pro or installing a HotFix which updates the version of Unity pro DTM library?

After installation, any eds file imported in Unity Pro catalog must be re-imported.

To avoid re-import, the following workaround can be used to keep DTM eds in the DTM catalog :
• Before Unity Pro or HotFix install : backup and save edslist.xml which is under \\ProgramData\Schneider Electric\Unity Pro Generic EtherNetIP DTM\Device Library
• After Unity Pro or HotFix install : install : Replace the new edslist.xml created after the installation by the backup of the edslist.xml.