Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the labels that fit with E-Stop ZB5AT8643M
With the stop of commercialization of the flat E-Stop label and the launching of 3D labels, there was no more solution for ZB5AT8643M
The product manager decided to create a few references of combined label + E-Stop
Here is the list of references that have been created (availability February 2017)
ZB5AT8643M130 = E-Stop ZB5AT8643M + Label ZBY9130 "ARRET D'URGENCE"
ZB5AT8643M140 = E-Stop ZB5AT8643M + Label ZBY9140 without marking
ZB5AT8643M230 = E-Stop ZB5AT8643M + Label ZBY9230 "NOT-HALT"
ZB5AT8643M330 = E-Stop ZB5AT8643M + Label ZBY9330 "EMERGENCY STOP"
ZB5AT8643M430 = E-Stop ZB5AT8643M + Label ZBY9430 "PARADA DE EMERGENCIA"
ZB5AT8643M630 = E-Stop ZB5AT8643M + Label ZBY9630 "ARRESTO DI EMERGENZA"