Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What version of Web designer support the BMXNOE0110 V6.3?

Issue

Web Designer V2.52 for BMXNOE0110 V6.3 only lets the user choose between V6.1 and V6.2









Product Line

M340, BMXNOE0110

Resolution


The current firmware version of the BMXNOE0110 is v6.3 but the web page version is still 6.2 (See Screenshot)


Because Web Designer is linked to the web page version and not the firmware version, when a BMXNOE0110 application is made, the customer needs to choose v6.2 if the module they have is v6.3 firmware in Web designer 2.52