Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many Modbus/TCP client connections can you have on the M221?
Issue:
How many Modbus/TCP client connections can you have on the M221?

Product Line:
Modicon M221, Modbus server, Modbus client

Resolution:
The M221 Ethernet as a Modbus TCP Server will support a maximum of 8 Client connections.