Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do I customize the display on the Altivar Process Drive?

Article available in these languages: Finnish

Issue:
How do I adjust/customize the main display on the Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive​

Resolution:



To adjust parameters on the top of the screen
- [My preferences] [Customization] [Param. Bar Select]

A
To adjust parameters in the middle of the startup screen
- [My preferences] [Customization] [Display Screen Type] [MPC]
C
B