Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV630- How do you set up the run command on DI1?
Issue:
ATV630 set up the run command on DI1.

Product Line:
ATV630

Environment:
2-wire control

Cause:
n/a

Resolution:
Suggest to go to menu 5.5 and set 2-wire control to 2-wire and set 2-wire type to Level.  This will automatically assign DI1 to run forward.