{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What do "angle compen", "ratio compen" mean for IEM3455?
If the  LVCT selected have the angle and ratio compensation values specified on it, the same needs to be configured into the meter with which it is used.

This clarification will be added in an upcoming release of iEM3000 user manual.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.