How can we help you today?

How to configure PME to work with HTTPS with SSL enabled?

Issue
Enabling SSL on the PME webpage and requiring HTTPS causes the webpage to no longer work.

Product Line

Power Monitoring Expert 8.2

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
Web Applications

Cause
The PME webpage uses hard coded HTTP links in the various web.config files. When the webpage is set to require HTTPS within IIS, the website breaks due to these links.

Resolution
The attached documents details the steps required to enable HTTPS with SSL encryption.

Recommendation

If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo.support@se.com

Support information

Schneider Electric Saudi Arabia

Attachment(s)
Host PME 8.2 over HTTPS with SSL enabled and HTTP Disabled (most secure)_revised.pdf [179.74 KB]
Host PME over HTTP and HTTPS with SSL enabled.pdf [221.05 KB]