Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you program an ATV630 for freewheel stop instead of ramp stop?
Issue:
Could not program an ATV630 for freewheel stop instead of ramp stop.

Product Line:
Altivar Machines, Altivar 630, Altivar 650

Environment:
All

Cause:
N/A

Resolution:
From main menu, go into menu 5 complete settings.
Go down to Generic Functions.  If you do not see this menu then please make sure to change access level under preferences to expert.
Find Stop configuration.
Set Type of Stop to freewheel stop.