Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Quantum 140NOE77101 hostname be changed?
Issue

Where the Host Name “140-NOE-771-01 Module” is being stored? Can it be changed?

Product Line

Quantum

Resolution

The Host Name “140-NOE-771-01 Module” is stored in the SNMP OID “System Name:” property.

The SNMP OID “System Name:” property is it read only, therefore, the hostname can’t be changed