Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I intend to monitor a system with RM35JA32MW relay at which the current comprises both the AC and DC components. Can the product function correctly?
YES, the product can function correctly.

Below is the front panel setting and waveform diagram.

Ti = Starting inhibit time delay adjustment potentiometer.

Function: On energisation, an inhibit time delay (1…20 s) makes it possible to inhibit (or ignore) current peaks on start-up of equipment.

You can try to adjust the RM35JA32MW product’s Ti setting to inhibit the inrush current during load start-up.