Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
At what temperature range can operate Schneider Electric servo motors?
BSH and BMH motors can work in temperature range -20°C to 40°C (more with derating). SH motors operation temperature is +5°C to 40°C (more with derating). The reason are mechanical tolerancies in bearings and the grease that does not work at low temperatures.