Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you capture a screenshot on the ATV630 and ATV930 process drives?
Issue:
Screenshot on the ATV630 and ATV930 process drive

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Wants to capture a picture of the screen on the ATV630 drive.

Resolution:
If you want to capture a screenshot on the ATV630 and ATV930 drives you will need to hold Function Keys 1 and 4 both at the same time.   The Screen will flash RED and blink indicating that the current screen was captured and saved into the HMIs memory.