Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you change the power identification of an ATV61?
Issue:
Needs to change the power identification of an ATV61

Product Line:
Altivar 61, ATV61

Environment:
all

Cause:
Can the power output of the drive be changed?

Resolution:
Power Identification is only available for the ATV61 drives.
Set Access level to Expert.
Go to Drive Menu > 1.4 Motor Control > Power Identification.  Power Identification should be IP20 for open style drives and IP00 for enclosed drives (E-Flex, M-Flex, MCC).
You'll need to hold Enter for 2 seconds in order to make this change.