{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: Battery Replacement for Back-UPS XS & RS LCD units.
Issue:
UPS indicates battery requires replacement.

Product Line:
  • BR1500LCD
  • BX1500LCD
  • BR1300LCD
  • BX1300LCD
  • BN1250LCD

Environment:
All Serial Numbers

Cause:
Failed selftest resulting in a need for battery replacement. UPS batteries require periodic replacement based on usage and operating environment.

Resolution:
The following video will provide details to removing and reconnecting the internal battery for the Back-UPS XS & RS LCD family of units.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.