Issue:
OPF1 fault on ATV320 Drive.
Product Line:
ATV320
Environment:
All
Cause:
NA
Resolution:
This fault is triggered when the drive detects one of the motor phases has been lost (or has very low current).
Check the connection between the drive and motor.
OPF1 fault on ATV320 Drive.
Product Line:
ATV320
Environment:
All
Cause:
NA
Resolution:
This fault is triggered when the drive detects one of the motor phases has been lost (or has very low current).
Check the connection between the drive and motor.
Released for:Schneider Electric Saudi Arabia