Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why can I not set my transient percentage below 105 for my ION 7650 meter?

Issue:
A customer is configuring the transient power quality setting and wants to use a percentage lower than 105.

Product Line:
ION 7650 meters

Environment:
ION Setup

Cause:
This is a restriction that is hard coded into the ION Transient Module.

Setup Assistant Transient settings

Resolution:
The lowest value which can be selected is 105% percent and the upper limit is 1000%.