Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the MTTF for the ATV630 and ATV930 process drives?

Article available in these languages: Japanese

Issue:
Mean Time to Failure (MTTF) for the ATV630 and ATV930 process drives.

Product Line:
Altivar ATV630 and ATV930 drives

Environment:
All

Cause:
Wants to know the MTTF or the MTBF rate on the ATV630 and ATV930 process drives.

Resolution:
See the attached document for the MTTF data.
Updated file IE7.0

Schneider Electric Saudi Arabia

Attachment(s)
Altivar Process MTTF_IE07.pdf [186.02 KB]