Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I run 2 ATV320 drives separately from 1 HMI?
Issue:
Can I run 2 ATV320 drives separately from 1 HMI?

Product Line:
ATV320

Environment:
All

Cause:
N/A

Resolution:
This can be done with a Magelis HMI using Modbus or other Serial Communication protocol that is supported by the ATV320.
The ATV320 remote keypad or HMI can only control 1 drive at a time.