Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV630 Process drive support BACnet communication?
Issue:
Is there a BACnet card for the ATV630 drive?

Product Line:
ATV600 series

Environment:
All

Cause:
N/A

Resolution:
Yes.  Order BACnet card part number VW3A3725.   Please be aware that the drive's firmware will need to be version 1.8 or higher.