Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EM4800 Control Power Voltage Range
Issue
Acceptable control voltage range for the EM4800

Product Line
EM4800

Resolution
The voltage range for the control power supply is 108VAC - 130VAC
Kindly contact triacta technical support for more information: