Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Search for and Open Unity Pro Sections using the Cross Reference Window?

Issue
How to Search for and Open Unity Pro Sections using the Cross Reference Window?

Product Line
Unity Pro , Control Expert

Resolution
Create a Unity Pro Variable (EBOOL or BOOL) with the same name as the Section and apply the Variable to the Section as the execution Control Variable.  Set the Initial Value of the Variable to True so the Section executes.

cross reference