Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV212 S-flex - What is the "output power percentage" scaled from?
Issue:
On the ATV212 series drive, "Output power" is displayed as a percentage.  What is the reference for this scale?

Product Line:
ATV212 series drives

Environment:
All models, All serial numbers.

Cause:
Information unavailable in current literature.

Resolution:
The Output Power percentage, as read over the network, is a percentage of the rating of the drive itself, not the motor.