Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have a Connexium offer for fiber distances greater than 32 kilometers?
Issue
Is there a Connexium offer for fiber distances greater than 32 kilometers?


Product Line
Connexium TCSESM103F2LG0
SFP TCSEAAF1LFH00

Environment
Windows 10


Resolution
The Connexium TCSESM103F2LG0 switches and TCSEAAF1LFH00 Gigabit fiber SFP's can be used.  These will support a distance of 24 to 72 Kilometers.

See attached documents for further information.

Schneider Electric Saudi Arabia

Attachment(s)
ConnexiumLongHaul.pdf [472.06 KB]