Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which explicit command is used to read the IP address of BMENOC0301, BMENOC0311 in Unity Pro ?
The IP address can be read by using explicit command Read_Var.
In the ADDM the address would be 'r.m.c.server address'
Here r is rack number, m is module slot of ENOC module, c is channel & server address is "100".
So the syntax would '0.3.0.100' where 3 is module slot and 100 is server address in the ENOC module.

Now to read the IP address the modbus data mapping is as follow : Address 40006 (IP1 & IP2) and Address 40007 (IP3 & IP4) :

mapping