Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does PWS mean on the Process Drive display?
Issue:
Customer cannot get their Process Drive to run.  Top line of the display reads status PWS.

Product line:
Altivar Process, ATV630, ATV930

Environment:
All

Cause:
SoMove connection

Resolution:
PWS indicates the drive Start/Stop is controlled by the SoMove software.  Commands to run from the external terminals or the keypad will not be taken into account.  The drive will still follow external analog signal.

Schneider Electric Saudi Arabia

Attachment(s)
PWS Capture.JPG.jpg [12.57 KB]