Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I prevent an ATV630 from running in reverse?
Issue:
How do I prevent an ATV630 series process drive from running in reverse?

Product Line:
ATV630 series

Environment:
All models, All serial numbers.

Cause:
Information difficult to find in user manual.

Resolution:
Under menu 5, Complete settings, navigate to sub menu 5.5, Command and Reference.  Locate the Reverse Disable parameter and set it to Yes.