Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Running Reconfigure on a system that has been configured for SSL breaks the SSL configuration

Issue:

Running Reconfigure on a system that has been configured for SSL breaks the SSL configuration

Product Line:

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment:

PME

Cause:

Running Reconfigure on a system that has been configured for SSL breaks the SSL configuration

Resolution:

It is possible to configure PME to use SSL - see FA309041.
If this has been done, and then the installer is run in Configure mode, duplicate entries are created in the ..\WebServices\web.config file. See below:

<service name="PowerQuality.Analytics">
<endpoint binding="webHttpBinding" contract="PowerQuality.Analytics" behaviorConfiguration="RESTBehavior" bindingConfiguration="http" />
<!--<endpoint binding="webHttpBinding" contract="PowerQuality.Analytics" behaviorConfiguration="RESTBehavior" bindingConfiguration="https" />-->
</service>
<service name="PowerQuality.EventProcessor">
<endpoint binding="webHttpBinding" contract="PowerQuality.EventProcessor" behaviorConfiguration="RESTBehavior" bindingConfiguration="http" />
<!--<endpoint binding="webHttpBinding" contract="PowerQuality.EventProcessor" behaviorConfiguration="RESTBehavior" bindingConfiguration="https" />-->
</service>
<service name="PowerQuality.DowntimeService.Impact">
<endpoint binding="webHttpBinding" contract="PowerQuality.DowntimeService.Impact" behaviorConfiguration="RESTBehavior" bindingConfiguration="http" />
<!--<endpoint binding="webHttpBinding" contract="PowerQuality.DowntimeService.Impact" behaviorConfiguration="RESTBehavior" bindingConfiguration="https" />-->
</service>

Should this happen, it will not be possible to log into the Web Applications. To correct this, it is necessary to repeat the steps required to configure PME for SSL.