Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I get the cable pin layout for the DeviceNet connector for the Altivar Process Drive?
Issue:
Cable pin layout for the DeviceNet connector for the Altivar Process Drive.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
Needs to know required cable connection pinouts

Resolution:

connector image