Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum allowable loss for BMXNRP0200?
Question:
What is the maximum allowable loss for BMXNRP0200 as as it can’t be located in the relevant datasheets.

Answer:
It is -45dB with regard to Asserted Loss of Signal.