Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an INFE fault on an ATV32 or ATV320 drive?
Issue:
INFE (Internal error 14 (CPU) fault on an ATV32 or ATV320 drive?

Product Line:
ATV320/ATV32 series drives.

Environment:
All models, All serial numbers.

Cause:
Customer does not have access to programming manual at current location.

Resolution:
The INFE indicates an internal problem with the CPU of the drive.  Either a ram, flash memory, or task fault.
To clear this fault, turn off all sources of power to the drive and wait for the display to go blank.
Wait at least 10 seconds and then re-apply power to the drive and use normally.
If the error returns, remove your control wiring from Logic, Analog, Relay contacts and communication network, one at a time, to determine if something is pulling down the supply or inducing noise.
If the problem returns or does not clear with the power cycle, please contact Product Support for further assistance.