Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to customize the appearance of Toolchest objects in Vijeo Designer

Issue:
I cannot find a way to change the color of the Toolchest objects in Vijeo Designer.

Product Line:
Vijeo Designer

Resolution:
Sometimes the appearance of the many Toolchest objects in Vijeo Designer are rather plain. Fortunately, there is a simple way to change the look to exactly what we want.

Take the CreateNew recipe button for example. It is simply a gray rectangular button. Very boring looking and colourless.

To keep the function of the button, and to make it appear nicer, simply overlay an image object on top. During runtime, when you touch the button with the new image on top, it will still function properly.