Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Realflo is Not Recognizing Newly Added Flow Runs

Problem:

An activation code has been used to increase the number of flow runs on a SCADAPack controller (let's say from 2 runs to 4 runs) but I am unable to load a configuration for the new number of flow runs.

Solution:

After applying the activation code to the controller, you can verify the options on the controller by selecting Controller > Flow Computer Information
Flow computer information window showing four flow runs are now activated

4 runs now appear to be activated. Now, if you try to install a new configuration with 4 flow runs configured, you could get an error message indicating that only 2 runs are available. Older versions of Realflo did not give much information when this error occurred which could lead to some confusion. Realflo 6.95.1 will now give you the following error.

Communication Status window error "The requested number of flow runs cannot be configured"

When the flow computer was first loaded to the controller, it looked at the number of enabled flow runs and allocated enough memory to accommodate only that number of flow runs (in this example, 2 flow runs).

To get past this problem in Realflo Expert Mode, go to Configuration > Replace Flow Computer and reinstall the flow computer. Realflo may try and install the most recent version of flow computer and it is up to the user to determine if a previous version is more appropriate for their application.

By replacing/updating the flow computer, Realflo will again look at the number of currently enabled flow runs (now 4) and allocate enough memory to handle up to 4 flow runs. With the new flow computer installed, you should now be able to load your configuration with up to 4 flow runs.

Note: This solution applies to SCADAPack, SCADAPack 32 and SCADAPack 300-series and does not apply to SCADAPack x70 controllers.