Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Example on how to use the real time clock in a Quantum non Unity PLC

Issue
Example of how to use the real-time clock in a Quantum non-Unity PLC

Product Line
Concept, ProWORX 32, ProWORX NxT

Environment
Windows 10

Resolution
No information can be found on how to use the registers for the real-time clock in the Concept application
for a Quantum PLC.

The attached document provides an example on how to use the real-time clock in a Quantum non-Unity PLC.

Schneider Electric Saudi Arabia

Attachment(s)
984 Real Time clock.pdf [41.54 KB]