Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the different part nos. of SCADAPACK inter module cables ?
These are the part numbers SCADAPACK inter-module cables.

Part NumberIntermodule cables
TBUM297269Shielded intermodule cable, 12 inches (0.3m) long
TBUM297192Shielded intermodule cable, 18 inches (0.45m) long
TBUM297193Shielded intermodule cable, 24 inches (0.61m) long
TBUM297192Shielded intermodule cable, 18 inches (0.45m) long
TBUM297131Shielded intermodule cable, 30 inches (0.76m) long
TBUM297162Shielded intermodule cable, 45 inches (1.14m) long
TBUM297174Shielded intermodule cable, 72 inches (1.82m) long
TBUM297162Shielded intermodule cable, 45 inches (1.14m) long