Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the A1U1 parameter not to show up in the Fr1 menu on the ATV320 drive?
Issue:
A1U1 parameter does not show up in the Fr1 menu on the ATV320 drive.

Product Line:
Altivar ATV320

Environment:
All

Cause:
Wants to setup the knob as the speed control

Resolution:
A1U1 will only show up in the Fr1 menu when you assign CHCF to SEP (Profile= Separate). Changing the value of this parameter requires holding the enter button for 2 seconds.

Schneider Electric Saudi Arabia

Attachment(s)
ATV320_programming_manual_EN_NVE41295_01.pdf [2.05 MB]