Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV630: How does Normal/Heavy duty affect the Current Limitation in the drive?
Issue:
ATV630 Normal/Heavy duty Current Limitation.

Product Line:
Altivar 630, ATV630

Environment:
All

Cause:
n/a

Resolution:
Go to menu 5.2 ( Motor Parameters), select Dual rating, then select:
Normal duty current limit is 1.1 of In
Heavy duty current limit is 1.5 of In.