Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity 11.1 and older returns 'STMSDK COM object initialization' error.
Product Line
Unity 11.1 and older

Environment
Windows 10

Resolution
Running older versions of Unity on a multi-core PC could cause the  "Error when initializing programming unit (STMSDK COM object initialization):
Unexpected exception (memory allocation, etc.). error to get returned.

This issue has been fixed in Unity 12.

It is recommended to update to Unity 12 or a version later to resolve the issue.