Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Connecting a Potentiometer to the ATV320 Drive
Issue:
Wiring a potentiometer to an ATV320

Product Line:
Altivar 320, ATV320

Cause:
Wiring and installation

Resolution:
Using the +10V source of the drive, hook up to +10, AI1, and COM.
AI1 terminal is middle (wiper) connection for a potentiometer.
+10 is the drive's 10Vdc source.
COM is neutral.