Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set the backlight timeout in the VW3A1111 keypad of AltivarProcess ATV900, ATV600?

Article available in these languages: Japanese

Issue:
How do you set the backlight timeout in the VW3A1111 keypad?

Product Line:
Altivar Process Drives using the VW3A1111 keypad

Environment:
All

Cause:
Preference

Resolution:
There is parameter for standby timeout in VW3A1111 with default value 60s. It is possible to set it to 'NO'. This parameter is stored in the remote keypad (not in drive). How to change it depends on the drive being used.

ATV32/ATV320:
Main menu -> interface -> Display config. -> LCD Settings -> Stand-by delay
Note: access level has to be set to expert

ATV630/ATV930/ATV340:
Main menu -> My preferences -> LCD settings ->Stand by

ATV61/ATV71
Main menu -> Display config. -> LCD Settings -> Stand-by delay
Note: access level has to be set to expert