Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How can one see the last fault that occurred on an ATS48 softstarter?
Issue:
Last fault occurred on an ATS48 Softstarter

Product Line:
Altistart 48

Environment:
All

Resolution:
Go into the SUP menu and select LFt parameter.  This will display the last fault that occurred on this drive.
The previous 4 faults can be accessed through SoMove software connected to the ATS48.