How can we help you today?

Using a password containing a combination of special characters can lock the user out of the NOE771xx module.

Issue
Using a password containing a combination of special characters can lock the user out of the NOE771xx module.

Product Line
140NOE77101 and 140NOE77111

Environment
Windows 10

Resolution
If you use a combination of special characters (e.g., ?@, etc.)  as part of the password,the module could lock the user out.

It is recommended not to use a combination of special characters in the password.


Schneider Electric Saudi Arabia