Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
After modifying a PowerSCADA Expert project, which steps must a user perform to make them active in Runtime.
Issue
After modifying a PowerSCADA Expert project, the user would like to know which steps must be taken to make them active in Runtime.

Product Line
PowerSCADA Operation 8.2
PowerSCADA Operation 9.0

Environment
PowerSCADA Expert Runtime

Resolution
Changes Being MadeCompileRestart
Client HMI
Reload
Alarm Server
Reload
Trend Server
Restart
I/O Server
Stop and Start
Schneider Electric Core Service Host
Modify existing graphics pages including embedded CicodeYesNoNoNoNoNo
Add completely new graphics page(s)YesYesNoNoNoNo
Changes to PowerSCADA users (by using Cicode runtime CreateUser function)NoNoNoNoNoNo
Changes to Active Directory group membershipNoNoNoNoNoNo
Changes to roles and Windows Active Directory group mappingYesNoNoNoYesNo
Changes to users and/or roles (by using the PowerSCADA Studio)YesNoNoNoYesNo
Changes to menu propertiesYesNoNoNoNoNo
Changes to server-side CicodeYesNoNoNoYesNo
Add/remove/modify alarm tagsYesNoYesNoYesYes (if you need to update immediately)
Add/remove/modify trend tagsYesNoNoYesNoYes (if you need to update immediately)
Add/remove/modify devices and/or variable tagsYesNoNoYesNoYes (if you need to update immediately)

Note: The above table is intended for PowerSCADA Expert 8.2. You may use the table as a reference for previous versions, however there has been no testing to validate these recommendations.