Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the smallest motor you can run on the ATV630 and ATV930 Process drives?

Article available in these languages: Spanish

Issue:
What is the rating for the smallest motor you can use on an Altivar Process Drive

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Wants to run a smaller motor on the larger drive.

Resolution:
The nominal motor current can be set to 25% of the drives current rating and the motor thermal can be set to 20% of the drives current ratings.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre