Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do I have to install a fuse protection upstream the A9E18327 ACTI9 IIL three-phase voltage indicator?
The A9E18327 is LED type indication light with a service life of 100,000 hrs. It does not need a protection by fuses. This control component is always meant to be connected downstream of a SCPD (short circuit protection device).

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre