Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M241 SD card specifications
Issue:
What are the M241 SD card specifications?

Product Line:
M241

Resolution:
You can use any SD card which is an SDSC or SDHC (High Capacity), up to 32 GB maximum memory and FAT32 file system formatted.