Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you connect the Multi-loader to a VW3A1101 keypad to get the saved files?
Issue:
Can you connect the Multi-loader to a VW3A1101 to get the saved files?

Product line:
VW3A8121, VW3A1101

Environment:
all

Cause:
Manual for the Multi-loader shows you can connect the device to the VW3A1101 keypads.

Resolution:
The connection is shown for the purpose of flashing an update to the keypad firmware using the VW3A8121 Multi-Loader.
The program files that are stored on the VW3A1101 cannot be loaded to the Multi-Loader because the format is different.