Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What’s the difference between Harsh and Coated modules for Modicon PAC products?

Question:
What’s the difference between Harsh and Coated modules for Modicon PAC products?

Answer:
In terms of protection level for severe environments as well as characters , they are same.
The only difference lies in the operating temperature.
Harsh module works at -25 °C~70°C while Coated module works at -25°C~60°C or 0°C ~60°C.