Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a replacement connector, mounting bracket, or grounding nut for an ION7650 or ION7550?

Issue
ION7650/7550 meter is missing one of its connectors

Product Line
ION7650 Meter
ION7550 Meter

Environment
Meter installation

Cause
A user may want to replace a lost, damaged, or missing connector, mounting bracket, or grounding nut for an ION7650 or ION7550

Resolution
There is a part number that can be ordered to replace any lost, damaged, or missing connectors, mounting brackets, or grounding nuts for ION7650 and ION7550 meters.
Part number FR-75XX-CONN is a spare connector kit containing all connectors, mounting brackets, and grounding nuts for FIVE ION7650 or ION7550 meters.

NOTE: the connector kit contains all connectors, mounting brackets, and grounding plugs for FIVE ION7650 or ION7550 meters.